Profit Growth Program
Signing up for the PGP program requires a commitment of the following to receive all the program benefits:
1. Co-load opportunity at 7,000 lbs (2 product categories minimum)2. In addition, if the co-load is 7,000 lbs and contains the following you will receive a 1% discount on the entire order
a. At least 1 core category (Steel, PVC, Cable or Strut)
b. At least 3 focus categories (Metal Framing Fittings, PVC Fittings, Wire Basket, Metal
Fittings, ETL-Verified PVC-Coated Conduit, ECN- Elbows, Couplings and
Nipples, Fiberglass, Flexible and Liquidtight Conduit) representing 10% of the
order dollar value
c. Order is placed via EDI
3. Bi-Annual Stock Rotation
a. Profit Centers will have a total return dollar amount based on 2% of their previous
year sales with Atkore
b. Zero re-stock fee
c. 2 annual stock rotation at the PC manager's discretion up to the determined
dollar amount
Any questions please contact:
Denis ChardacVP of Strategic Accounts
dchardac@atkore.com
Phone: 678-850-7680